What is the intended use case for the digital filter on the I/O pins of the S32K1xx MCUs? It can delay the input for up to 31 clock cycles, but that is too small to be a debouncer for a push button (with the clock running from any source except for the 32kHz source), so it seems an external schmitt trigger or a software debouncer is needed for that. Is my understanding correct?
Also, on an unrelated note, when I access the NXP forums all the titles are in some Asian language; only the user generated code is in English (I am accessing this from the United States). This makes it cumbersome to use the site. I use Chrome running on Windows 11, but I have noticed the same behavior with Internet explorer as well.
解決済! 解決策の投稿を見る。
Hi@durga_choudhury
yes, your understanding is correct.
The digital filter can delay input transitions by up to 31 clock cycles, which is useful for:
This is especially helpful for high-frequency signals or noisy environments, where short spikes could cause false triggering.
Use the digital filter for high-speed signal cleanup, like encoder inputs or external interrupts from fast peripherals.
For push buttons, rely on:
The language of the webpage can be changed after logging in. This should be related to your IP location, but I am not sure about the details.
Hi@durga_choudhury
yes, your understanding is correct.
The digital filter can delay input transitions by up to 31 clock cycles, which is useful for:
This is especially helpful for high-frequency signals or noisy environments, where short spikes could cause false triggering.
Use the digital filter for high-speed signal cleanup, like encoder inputs or external interrupts from fast peripherals.
For push buttons, rely on:
The language of the webpage can be changed after logging in. This should be related to your IP location, but I am not sure about the details.