Hello, I am trying to make a simple board with just the S32K341EHT0MPAST on it and some pins to access some analog and digital i/o and the i2c.
However looking at the reference manual and it seems like every GPIO pin is extremely multifunctional? I'm a bit overwhelmed and I don't understand how you would set each pin to a specific function. There are so many "ALTx" columns.
I see on the attached excel file for the s32k3 series that pin 41 and 42 are LPI2C1_SCL and LPI2C1_SDA respectively, and that there is another set of LPI2C0 pins. Do I understand correctly that I should be fine to use pin 41 and 42 as SDA and SCL and that the I2C0 is another "set" of i2c pins I could access?

For simple digital and analog i/o I'm also a little lost, I see ADC_Sx as "standard input" pins available, but for digital would those be FXIO_Dx pins?