Hello,
I am implementing a project on S32K144 using the S32DS IDE v3.4, when I use the "round" function and build the project I get the error :
even though I made sure to include the math.h libraryany reason for that ?
Thank you.
已解决! 转到解答。
Hi,
math.h is only header file for math library. You need to add libm.a library into your project in project properties:
在原帖中查看解决方案
Is there a similar solution for the imxrt1176
I am getting a similar error this is the embedded coder window
The exact error from the diagnostic window
I'm not familiar with imxrt1176 and it's development tool, but the principle is very same. You need add math library and let the linker know where the library archive is (library path - if it is not already configured).