Unable to configure all ports for S32K3X8CVB with TJA1103 and the GMAC Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to configure all ports for S32K3X8CVB with TJA1103 and the GMAC Driver

454 Views
BenjaminKubitschek
Contributor I

Hi,

I try to get to run your Eth_43_GMAC_TS_T40D34M30I0R0 driver on the S32K3X8CVB with the TJA1103 development board. For this I configured the ports like it is descriped in the UserManual of the CVB:

BenjaminKubitschek_0-1688445405467.png

 

But for the ports PTD13, PTD14, PTB2, PTB20, PTB21 and PTA26 I am not able to configure the correct PortPin Mode.

E.g. for the PTD13 Port in the UserManual there is the signal "ENET_INH_LS" mapped to the port, what ever this signal is. Anyway, in the port module I do not finde any mode which could be meant here, at least not by name:


BenjaminKubitschek_1-1688445823678.png

BenjaminKubitschek_2-1688445834274.png

 

BenjaminKubitschek_3-1688445842823.png

 

Another question: Is for the Ports PTB2, PTB20, PTB21 and PTA26 is there the SPI module needed for? Also for them I do not finde the correct Pin-Mode in the Port-Module configuration.

Could you please help me with this?

 

Thank you,

Benjamin Kubitschek

 

 

0 Kudos
Reply
1 Reply

435 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @BenjaminKubitschek 

S32K3X8EVB-Q289 is still not available for the mass market. The information of it is not public, and I am not able to check and verify it as I do not have the information due to the security levels when working with an automotive part such as this.

If you are already working with the S32K3X8EVB-Q289, I believe you should already have a contact that helped you get the information, could you please contact that person for further support on this part?

 

B.R.

VaneB

0 Kudos
Reply