Hi,
could you please specify the S32K148EVB version you have?
Also which SDK version did you select when creating can_pal example?
BR, Petr
Dear Petr,
Thanks for your reply,
Firstly,about your concern:
S32K148EVB version:S32K148EVB-Q176 2017 NXP B.V.
SDK version:0.8.6
I added a test code on can_pal example that send 0x55 with LPSPI1 channel recurrently,I run this test for monitor the SPI waveform,then I got the test result as shown as below:
(1)Waveform SBC_SPI_CLK on oscilloscope channel 1,take R554 as test point;
(2)Waveform SBC_SPI_MOSI on on oscilloscope channel 2,take R563 as test point.
Waveform SBC_SPI_MOSI is abnormal compared with 0x55,it seems like the hardware issue? I got the same test result on two S32K148EVB boards.
So,do you have any other advices?Thank you.