UART continuous transmission with interrups [AsyncSend/SetTxBuffer ]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART continuous transmission with interrups [AsyncSend/SetTxBuffer ]

1,072件の閲覧回数
JorgeSans
Contributor II
 

Hello,

I am trying to program an application for an S32K311 with continuous reception and transmission using the following functions:

  • Lpuart_Uart_Ip_AsyncSend
  • Lpuart_Uart_Ip_SetTxBuffer
  • Lpuart_Uart_Ip_GetTransmitStatus

 

  • Lpuart_Uart_Ip_AsyncReceive
  • Lpuart_Uart_Ip_SetRxBuffer
  • Lpuart_Uart_Ip_GetReceiveStatus

As well as a callback function to receive events of type Lpuart_Uart_Ip_EventType.

I have managed to get the reception part working correctly, but the transmission part is not working as expected.

Could someone explain how the functions dedicated to transmission should be used and ideally provide an example application?

0 件の賞賛
返信
3 返答(返信)

1,031件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @JorgeSans,

I'm afraid there is no such example.

Can you describe the issue and share you code here?

 

Thank you,

BR, Daniel

0 件の賞賛
返信

1,016件の閲覧回数
JorgeSans
Contributor II

Hi @danielmartynek 

 

As I haven't been able to find the correct way to use the transmission mode with interrupts without resorting to blocking calls, I am temporarily using them. To prevent the start of a new message transmission before the previous one is finished, I create a lock. However, this is not ideal when the goal is to avoid blocking the application's execution.

What I need is to find an analogous method to the reception process, which works excellently with interrupts.

Any suggestions on how this should be implemented?

#include "SerialFacility.h"
#include <string.h>
#include "cmsis_gcc.h"

extern Queue_t commandQueue;
uint8_t rxCommandBuff[CMD_BUFF_RX] = { 0 };
volatile uint8_t cursor;

void serialFacilityInit( ){
  	// Initializes an UART driver with interrupt enabled
    IntCtrl_Ip_EnableIrq(LPUART3_IRQn);
    // Configure UART3 peripheral
	Lpuart_Uart_Ip_Init(UART_CHANNEL_3, &Lpuart_Uart_Ip_xHwConfigPB_3);

	//  Start reception of command in interrupt mode
	Lpuart_Uart_Ip_AsyncReceive(UART_CHANNEL_3, rxCommandBuff, 1);
}

void uart3EventCallBack( const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData ){

	if (HwInstance == UART_CHANNEL_3)
	{
		if(Event == LPUART_UART_IP_EVENT_RX_FULL)
		{
			// The reception stops when newline is received or the buffer is full
			if ( ( rxCommandBuff[cursor] != FRAME_DELIMITER ) && ( cursor != ( CMD_BUFF_RX - 2U ) ) )
			{
				// Update the buffer index and the rx buffer
				cursor++;
				Lpuart_Uart_Ip_SetRxBuffer(UART_CHANNEL_3, &rxCommandBuff[cursor],1U);
			}
			else
			{
				EnqueuedCommand pendingCmd;
				memcpy( ( char* ) pendingCmd.commnddBuff, ( char* ) rxCommandBuff, cursor );
				// Adding end of string dekimitator
				pendingCmd.commnddBuff[cursor] = '\0';
				pendingCmd.commandSize = cursor;
				if (!q_isFull(&commandQueue)) {
					q_push(&commandQueue, &pendingCmd);
				}
				cursor = 0;
				Lpuart_Uart_Ip_SetRxBuffer(UART_CHANNEL_3,&rxCommandBuff[cursor],1U);
			};
		}
		else if(Event == LPUART_UART_IP_EVENT_END_TRANSFER)
		{
			// Enable interrupt for again to be able to continue receiving data
			Lpuart_Uart_Ip_AsyncReceive( UART_CHANNEL_3, rxCommandBuff, 1 );
		}
		else if( Event == LPUART_UART_IP_EVENT_END_TRANSFER )
		{
					// Implementatio here to handl continous trasnmission
		}
	}
}


void sendMessage( const uint8_t* message )
{
	size_t length = strlen( ( char * ) message );
	volatile Lpuart_Uart_Ip_StatusType lpuartStatus = LPUART_UART_IP_STATUS_ERROR;

	lpuartStatus = Lpuart_Uart_Ip_AsyncSend(UART_CHANNEL_3, message, length);
        // Temporaru solution to avoid trasnmitinf a new  message before ending current trassmission
	uint32_t remainingByte;
	do
	{
		lpuartStatus = Lpuart_Uart_Ip_GetTransmitStatus(UART_CHANNEL_3, &remainingByte);
	    // Waiting for the transmit  to be completed
	} while ( remainingByte > 0 );
}

 

タグ(2)
0 件の賞賛
返信

1,006件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信