Trying to install the S32SDK_S32K1xx_RTM_4.0.2 SDK extension through the S32 Design Studio IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trying to install the S32SDK_S32K1xx_RTM_4.0.2 SDK extension through the S32 Design Studio IDE

1,406 Views
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to install the S32SDK_S32K1xx_RTM_4.0.2 SDK extension through the S32 Design Studio IDE, but I am getting an error. Please help me install it.

Please refer to the attached screenshot. provide the solution ASAP.

0 Kudos
Reply
7 Replies

1,402 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It is recommended to install S32K1 RTD 2.0.x with S32DS Extensions and Updates in S32DS v3.5.  If the online installation fails, please refer to HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5
 
Or install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.
It is not recommended to install S32K1 SDK 4.0.x in S32DS v3.5According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.x into S32DS 3.5 or above version.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,396 Views
Anilpatil_SasvaAuto
Contributor III
Trying to Install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4. But getting error
0 Kudos
Reply

1,369 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm afraid you need to offline install the S32K1xx development package:

Download S32 Design Studio 3.4 S32K1xx Service Pack 1 (SW32K1_S32DS_3.4.1_D2106.zip) at My NXP Account -> Software Licensing and Support -> Software accounts and add it as an updated site.

S32 Design Studio 3.4 S32K1xx Service Pack 1 SW32K1_S32DS_3.4.1_D2106.png

Help Install New Software.png

install SW32K1_S32DS_3.4.1_D2106.png

0 Kudos
Reply

1,364 Views
Anilpatil_SasvaAuto
Contributor III
I want to install install the S32SDK_S32K1xx_RTM_4.0.2 SDK as well it is important for me
0 Kudos
Reply

1,361 Views
Anilpatil_SasvaAuto
Contributor III
I apologize for the error; I mistakenly typed 4.0.2. I want to install the S32SDK_S32K1xx_RTM_4.0.3 SDK. Please help me.
0 Kudos
Reply

1,334 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

After you have installed SW32K1_S32DS_3.4.1_D2106.zip offline, you should be able to install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.

install S32SDK S32K1XX RTM 4.0.3 online via S32DS Extensions and Updates.png

0 Kudos
Reply

1,362 Views
Anilpatil_SasvaAuto
Contributor III
This is not include the S32SDK_S32K1xx_RTM_4.0.2 SDK
0 Kudos
Reply