The problem of files which CT configuration generate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem of files which CT configuration generate

4,872 Views
Hermit
Contributor I

Hi Team

We team want to develop the project on S32K342. The version of IDE is S32DS V3.5 and the package of RTD is "SW32K3_RTD_4.4_2.0.2_DS_updatesite_D2211.zip". I attach a creenshot which shows the specific version I set up. 

When we have finished the CT configuration and updated the code, we can not build it successfully. One of attached screenshots shows the problem. And we find that the content of it is totally same with another head file. If we replace "FlexCAN_Ip_Sa_BOARD_InitPeripherals_PBcfg.h" with "FlexCAN_Ip_Sa_PBcfg.h",it can be built successfully.

Does the RTD version matter?

 

Best Regards

Hermit

0 Kudos
Reply
2 Replies

4,861 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Hermit,

Below is my test result, everything works fine.

Senlent_0-1675414717257.png

The RTD 2.0.2 FlexCAN module does not generate the file "FlexCAN_Ip_Sa_PBcfg.h".

0 Kudos
Reply

4,834 Views
Hermit
Contributor I

Hi Senlent

Thanks for your response.

Best Regards,

Hermit

0 Kudos
Reply