The issue of the FLS module not being included in S32K3 RTD 4.0.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The issue of the FLS module not being included in S32K3 RTD 4.0.

271 Views
gumu
Contributor IV

Dear Sir,

Recently, when I was using RTD 4.0, I found that the FLS module was not available for selection in a new project. The version I installed is: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip. Screenshot below:

gumu_0-1716788399718.png

Is it possible that the FLS module in the new version of RTD has been replaced by INFLS and EXFLS modules?

Thanks!

Tags (1)
0 Kudos
Reply
1 Reply

250 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Because this RTD is based on AUTOSAR R21-11, there is no FLS module.

Please refer to the discussion in no fee and fls modules in RTD of s32k3x


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply