The all-new S32K116 must be swiped by Jflash once before it can be debugged using S32DS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The all-new S32K116 must be swiped by Jflash once before it can be debugged using S32DS?

341 Views
phidiawang
Contributor III

Hi,

   I found that the new S32K116 chip must be swiped by Jflash once before it can be debugged using S32DS,is right?

0 Kudos
1 Reply

327 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,
these microcontrollers are shipped with fully erased flash, only flash security byte in flash configuration field is programmed to unsecure state 0xFE. So, the devices are ready to use and no special action is needed. It's not even necessary to erase them first, those can be programmed directly. In production, the devices can be re-erased anyway to achieve highest possible data retention which starts counting from erase operation.
Regards,
Lukas

0 Kudos