The S32K3 secure boot (HSE_FW) is not working properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The S32K3 secure boot (HSE_FW) is not working properly

ソリューションへジャンプ
21,306件の閲覧回数
luhaiou_autolink
Contributor I

I encountered the following problems when debugging Advanced_SecureBoot Project, please help support.

my project test on s32k312.

1.The Secure Boot CFG result is as follows

luhaiou_1-1705058078123.jpeg

2. I change to secure boot by setting BOOT_SEQ

luhaiou_2-1705058359708.png

but ,my app can not be boot,Please help analyze the reason, thank you very much

 

0 件の賞賛
返信
1 解決策
19,897件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

I checked this situation and I detected that the CMAC tag value has not been updated yet at the address 0x584000.

Pass:

nxf78987_0-1708918667569.png

Fail:

nxf78987_1-1708919480401.png

Best regards,

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
20 返答(返信)
21,130件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

1. Did you define IVT_BOOT_CFG_WORD_BOOT_SEQ correct as below?

    #define IVT_BOOT_CFG_WORD_BOOT_SEQ  (1 << 3)

2. Did you implement Advanced_SecureBootps steps correct?

nxf78987_0-1705659562720.png

 

Best regards,

Dan

0 件の賞賛
返信
21,120件の閲覧回数
luhaiou_autolink
Contributor I

 

1. Did you define IVT_BOOT_CFG_WORD_BOOT_SEQ correct as below?

    #define IVT_BOOT_CFG_WORD_BOOT_SEQ  (1 << 3)

Yes.

After the Secure Boot configuration was completed, I set the BOOT_SEQ bit and re-downloaded it to the MCU,

but ,my app can not be secure boot.

luhaiou_autolink_1-1705660994128.pngluhaiou_autolink_2-1705661063612.png

 

2. Did you implement Advanced_SecureBootps steps correct?

Each step of the configuration Advanced_SecureBoot has a corresponding log output

You can refer to the main.c .text file.

luhaiou_autolink_0-1705662728990.png

 

My project was tested on the s32k312,

The versions of HSE_FW and SBAF are shown in the figure below

luhaiou_autolink_1-1705662771411.png

 

My demo is based on the following example provided by NXP,

SW745310-SecureBootAppNoteDemo(1.0)

S32K3_HSE_DemoExamples.exe

 

 

0 件の賞賛
返信
21,046件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

Following the Secure Boot project of NXP, the IVT was updated by code instead of adding IVT_BOOT_CFG_WORD_BOOT_SEQ into the ivt_flash array as your code. And maybe, this caused your program boot to fail.

From my point of view, you should remove IVT_BOOT_CFG_WORD_BOOT_SEQ and update IVT as the sample project of NXP.

nxf78987_1-1705920701828.png

nxf78987_0-1705920664190.png

Best regards,

Dan

0 件の賞賛
返信
21,024件の閲覧回数
luhaiou_autolink
Contributor I

Thanks for your suggestion,

1. I've tried this way, and when modifying the IVT_0,

UpdateIvt( BLOCK0_IVT_ADDRESS, BLOCK0_IVT_ADDRESS, SECURE_IVT ),

this step produces hard_fault, probably the flash access function is restricted when accessing the same FLASH BLOCK.

You can try debugging on the same hardware platform (s32k312), and using the same software platform (SBAF: 0.13.0.0.8.0, HSE_FW: 0.13.0.1.2.1), thank you very much

2.Refer to the demo S32K344_Advanced_SecureBoot in the S32K3_HSE_DemoExamples.exe,

and also does not update the IVT through code, but directly modifies the IVT and then compiles and downloads it

luhaiou_autolink_0-1705979870246.png

 

0 件の賞賛
返信
20,946件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

Could you send me your securebootConfig project?

I'm going to check from my side.

Best regards,

Dan

0 件の賞賛
返信
20,929件の閲覧回数
luhaiou_autolink
Contributor I

My project refers to SW745310-SecureBootAppNoteDemo (1.0),

SW745310-SecureBootAppNoteDemo (1.0) is from NXP ,

and requires a non-disclosure agreement (NDA) before it can be downloaded.

So it's not appropriate for me to put my project directly in a public forum.

I can provide you with the project, but you see what is the best way to do it.

0 件の賞賛
返信
20,918件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

Could you send your project to me via email?

I'm going to send you my email in the message.

Best regards,

Dan

0 件の賞賛
返信
20,794件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

I used the S32K312EVB board to test your project with some modifications related to updating the IVT by code as below steps:

Step 1: Uncomment updateIvt statements.

nxf78987_0-1706691365417.png

Step 2: Put C40_Ip function on RAM by actions:

2.1 Replace C40_Ip.c and C40_Ip.h file by these files in the S32K312_SecureBootCfg_EVBQ172_201_350_FW0210 project.

2.2: Comment line 1970 in the C40_Ip_MainInterfaceHVJobStatus() function in the C40_Ip.c file because the OsIf_GetElapsed() function will be put on Flash.

nxf78987_1-1706691653646.png

After do the above steps, I link my application in the linker in your project.

Next, I debug your project on S32DS and when the program configured secure boot completed, I caused a functional reset by pressing reset button (SW3) then application was performed (green led was blinking and the smrstatus[0] and smrstatus[1] both equal to 1 - secure boot was performed successful).

This is the log of cl_factory_s32k312_hse_fw_install project:

nxf78987_2-1706694436684.png

And this is log of secure boot application (after I pressed reset button).

nxf78987_3-1706694559679.png

The above image indicated that the advanced secure boot was performed successful.

I'm going to send your project modified and my secure boot application via email.

Best regards,

Dan

0 件の賞賛
返信
20,748件の閲覧回数
luhaiou_autolink
Contributor I

Hello Dan,

I've fetched your project, thank you very much.

Putting the flash access code in ram solves the RWW (ready while write) problem of FLASH,

and your modification to the flash driver is very useful for me.

But the problem I mentioned in my last email needs your help to solve.

It may be that the description in the last email was not detailed enough, so I will describe the problem in detail again.

  The demo I provided to you will successfully implement the SecureBoot configuration and jump to the app successfully.

The problem is that when the configuration is completed and the app is successfully launched,

when you use PE online debugging again, it will cause the HSE_FW to work abnormally,

and it feels like the previously installed key is corrupted, and you have to reformat the key catlog and reinstall the key.

The video file I provided earlier,2024-01-29-16-12-29.mp4,The main operation process is:

cfg(with BOOT_SEQ = 1)->reset->app boot successfully->modyfy cfg project->debug again->HSE_FW fail

You can also replicate this phenomenon in your own projects.

1.Uncomment

luhaiou_autolink_0-1706768618658.png

2.debug again with PE,it will stop here

luhaiou_autolink_1-1706768765882.png

 

0 件の賞賛
返信
20,737件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

To solve this issue, please add two statements into else as below:

nxf78987_0-1706773171152.png

Best regards,

Dan

0 件の賞賛
返信
20,625件の閲覧回数
luhaiou_autolink
Contributor I

There is also a doubt about Advance Secure Boot, which involves the design of our software architecture.

Our products need to realize the upgrade function of APP. Our software is designed to configure the Advance Secure Boot while the product is in the factory.

After that, we provide an app upgrade package to replace the original app, and our upgrade package is with Cmac_tag.

luhaiou_autolink_0-1706949123074.png

cmac_tag_first,cmac_tag_new1,cmac_tag_new2,,, are different.

However, after updating the app_new and cmac_tag_new, I can't start the app normally.

I personally understand that when installing SmrEntry, the important information is the smr_src, smr_size, key_handle, authentication scheme, cmac_tag_pointer and legth.

I have always understood that cmac_tag_pointer is provided with location information, and the specific content of this location can be different, as long as it matches the calculation result of the corresponding region content.

If the HSE_FW also records the specific content of the cmac_tag_pointer, then the SMR entry must be reconfigured for each APP upgrade, which is too inflexible.

I hope my understanding is wrong, and I look forward to hearing from you,

Here's how I tested it:

1.Create new branch 

1.1 new branch of cl_factory_s32k312_hse_app0_blinky Project

luhaiou_autolink_1-1706950991209.png

1.2 new branch of cl_factory_s32k312_hse_fw_install Project

luhaiou_autolink_2-1706951101292.png

2.modify cl_factory_s32k312_hse_app0_blinky Project

2.1.modify cl_factory_s32k312_hse_app0_blinky ld file

luhaiou_autolink_3-1706951837618.png

2.2 modify main.c

luhaiou_autolink_4-1706952056129.png

main.c of cl_factory_s32k312_hse_app0_blinky is shared with cl_factory_s32k312_hse_fw_install ,Store in cl_factory_s32k312_hse_fw_install projectif you  use git,pay attention to it

3.Get app_new de cmac_tag

3.1 compile cl_factory_s32k312_hse_app0_blinky 

3.2compile cl_factory_s32k312_hse_fw_install 

3.3 debug cl_factory_s32k312_hse_fw_install , get  cmac_tag in  log

luhaiou_autolink_5-1706953142655.png

3.4 modify main.c with cmac_tag in step 3.3

luhaiou_autolink_7-1706953227136.png

4.Debugging app_new

4.1 compile cl_factory_s32k312_hse_app0_blinky 

4.2compile cl_factory_s32k312_hse_fw_install 

4.3Debug cl_factory_s32k312_hse_fw_install 

APP_boot ok,

Now, cl_factory_s32k312_hse_app0_blinky.hex  image is with cmac_tag,Save this file

luhaiou_autolink_8-1706953617951.png

5. Both projects return to the original branch and recompile and run,

Up to now, the image in the MCU is called app_first, and then update the app_new directly (the image saved in step 4.3)

Then app_new can not boot successfully

0 件の賞賛
返信
20,709件の閲覧回数
luhaiou_autolink
Contributor I

That's awesome,

I tried the method you provided and it solved the problem, thank you very much.

I still have one more question I would like to continue to ask,

When I didn't add  two statements into else, why is the damage to the hse_fw irreversible,

At this time I didn't make any changes to the HSE_FW and key catlog,

when I reset again, it should jump directly to the app, which is the normal logic,

The actual phenomenon is that the MCU can never return to normal.

You can see this permanent destruction after making the following modifications,

luhaiou_autolink_1-1706846015692.png

 

 

 

0 件の賞賛
返信
20,197件の閲覧回数
luhaiou_autolink
Contributor I

The above 2 comments, is there any new progress,

I am very much looking forward to your reply,

thank you very much

0 件の賞賛
返信
20,152件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

I realized that you configured int_flash area to overlap the int_flash_cmac_tag area in your application and maybe the cmac tag area can be modified.

nxf78987_0-1708428686475.png

You have to ensure that there are no areas that can overlap and can modify cmac_tag area.

Best regards,

Dan

0 件の賞賛
返信
20,144件の閲覧回数
luhaiou_autolink
Contributor I

Thank you for your reply to my queries,

int_flash_cmac_tag is not overlap,

We can confirm the file from cl_factory_s32k312_hse_app0_blinky.hex  in new branch

luhaiou_autolink_0-1708430817391.png

1.I would like to ask you to confirm that when using Advance secure boot, when the app is updated, the user will have to reinstall the SMR in order to store the new auth-proof to HSE Secure NVM.

May be auth-proof is stored directly in the HSE Secure NVM instead of storing the proof address in the codeflash.

This may be the functional feature of ASB mode?

0 件の賞賛
返信
20,096件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

I asked the FAE team about your question and they said that:

the auth proof is mostly on the normal code flash.

but they have tried just update auth tag before when using the secure boot demo, it works fine, you can try the same process on the demo first.

Best regards,

Dan

0 件の賞賛
返信
19,974件の閲覧回数
luhaiou_autolink
Contributor I

hello .@dan

Thank you for your long support,

The reason for the Secure Boot failure after updating the app has been found,

the last step , When installing the new_app, the entire chip is wiped and the IVT area is also erased,

so boot fail !

Now there is only one problem left unsolved,This issue still needs your help

luhaiou_autolink_0-1708690640743.png

 

0 件の賞賛
返信
19,223件の閲覧回数
anakha
Contributor III

Hi @luhaiou_autolink,
Did you solve this problem? if yes how?

0 件の賞賛
返信
19,214件の閲覧回数
luhaiou
Contributor II

Yes,In my project, Secure Boot works fine.

There are many problems in the process

It is recommended to directly use the demo provided by the official to implement the functions first, and then adapt to your own project step by step.

You can get the demo here.

S32K3 - NXP Community

0 件の賞賛
返信
19,898件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @luhaiou_autolink,

I checked this situation and I detected that the CMAC tag value has not been updated yet at the address 0x584000.

Pass:

nxf78987_0-1708918667569.png

Fail:

nxf78987_1-1708919480401.png

Best regards,

Dan

0 件の賞賛
返信