Hi,
In the RM of FlexCAN , the documentation says that the data frame contains CRC check, but as far as the program is concerned, it does not show. How do I verify the CRC check error interrupt?
Thanks!
Hi SONGTAOSI,
About how S32K1's FlexCAN detects CRC errors, please refer to About error and status register 1
About how to generate wrong CAN frames: If you have PCAN, you can refer to PCAN-View Error Generator - User Guide. If not, you can refer to: Configurable Error Generator for Controller Area
Network
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------