Dear All,
I have some questions about CSEc secour boot:
1.I want to protect the application code,the code address must from address 0x00000000?Can i modify the start address?
2.Is there a conflict between EEP Init and CSEC_DRV_Init?
Hello @wang_q4,
Please refer to the RM rev.13, Section 36.5.13.25 CMD_BOOT_DEFINE.
Which drivers do you use? What do you mean by EEP Init?
Regards,
Daniel