Secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,538件の閲覧回数
972276616
Contributor II

Hi,

After developing boot code on S32K116 development board,I want to use the CSEC module in SDK to check bootloader for integrity and authenticity.

Is there a CSEC module check BootLoader code use routine as a reference?

 

thank you

Best wishes

zheng

0 件の賞賛
返信
1 解決策
3,531件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Zheng,

There is csec_boot_protect_s32k118 SDK example, so you can refer to that.

Please read the csec_boot_protection.dox description:

danielmartynek_0-1610107421918.png

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,044件の閲覧回数
Gideon
Contributor III

Where can i download the  csec_boot_protect_s32k118 SDK example ?

0 件の賞賛
返信
2,028件の閲覧回数
Gideon
Contributor III

I have found the the example.

when you setup the SDK S32 Design Studio for S32 Platform 3.4 

the example in the path:

C:\NXP\S32DS.3.4\S32DS\examples

 

0 件の賞賛
返信
3,532件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Zheng,

There is csec_boot_protect_s32k118 SDK example, so you can refer to that.

Please read the csec_boot_protection.dox description:

danielmartynek_0-1610107421918.png

 

Regards,

Daniel

0 件の賞賛
返信