I created a S32K344 Project. which files are need to be saved in source control?
For sure the .mex file is required and the generated files would not be need as they can easily be recreated.
My guess is as follows. Can someone confirm this?
Save; .mex and all files at this top level. /src, /includes, /Project Settings
don't save; /RTD, /board, /generate, /Debug_Flash (or the equivalent in RAM or release), /RemoteSystemsTempFiles
not sure; /.settings, /.metadata, /.metadata/plugins
已解决! 转到解答。
Hi @ekmas-19,
For both the save and don't save list, I agree.
For not sure, I recommend keeping /.project, /.cproject and /.settings, in order to import/build the project without reconfiguring it manually (for compiler and CDT configurations).
You can ignore /.metadata, as it normally includes workspace related configuration.
Keep in mind that, for reproducible builds, the same RTD version (with patch) must be used.
Best regards,
Julián
Hi @ekmas-19,
For both the save and don't save list, I agree.
For not sure, I recommend keeping /.project, /.cproject and /.settings, in order to import/build the project without reconfiguring it manually (for compiler and CDT configurations).
You can ignore /.metadata, as it normally includes workspace related configuration.
Keep in mind that, for reproducible builds, the same RTD version (with patch) must be used.
Best regards,
Julián