SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SW32K3_RTD_4.4_1.0.0_DS_updatesite_D2110

1,662 Views
Venkatesh_Vedula
Contributor I

Hi,

I'm facing issue after updating RTD drivers in S32DS which you have released on 07-oct-2021. After importing an example code into project, I used to update the code in .mex file. But post update, I'm getting some errors in Drivers as well as in MCAL drivers. Some of the errors I'm posting here.

Errors:

Issue: Mcu not found in the toolchain/IDE project. Project will not compile!

Issue: mcl not found in the toolchain/IDE project. Project will not compile!

Issue: port not found in the toolchain/IDE project. Project will not compile!

Issue: Platform not found in the toolchain/IDE project. Project will not compile!

And also I'm unable to see RTD source folder in the project which was automatically added after importing the project in the previous version.

Thank you,

Venkatesh

 

 

Tags (1)
0 Kudos
2 Replies

1,610 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Venkatesh_Vedula ,

 

I have checked this case and I found that this issue happen because the S32DS has not installed the new development package. Unfortunately this development package was not published in NXP website yet. I am asking our team to do it. I will let you know if any update.

 

Best regards,

Hung

0 Kudos

1,595 Views
Venkatesh_Vedula
Contributor I

Hi @hungnguyenphi,

Thanks for the information. Please let me know when the update is available.

Regards,

Venkatesh Vedula

0 Kudos