STM cannot work in S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

STM cannot work in S32K344

523件の閲覧回数
Harryzhou
NXP Employee
NXP Employee

Hello,

Now I am developping the STM module of S32K344. I have some trouble.

I make sure I have set the clock source for STM0 and STM1. The clock is 40MHz from FXOSC. But I cannot set the value of related registers. The code is error when go till setting registers, such as "STM_0->CR |= STM_CR_CPS(0);". I have no idea to figure that.

I just set the system clock and core clock. But I'm not sure is the configuration is correct.  When I set GPIO to output high, it works. 

 

Thanks!

Best Regards,
Harry Zhou
0 件の賞賛
0 返答(返信)