SPI, ADC and PWM pin configuration queries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI, ADC and PWM pin configuration queries

504件の閲覧回数
Fasil1
Contributor I

image.png

Attached is a snapshot from S32K3xx datasheet regarding ADC channels and PWM. Is this same configuration applicable for S32K312? For example: ADC0: 16 channels at 400Hz and ADC1: 4 channels at 20kHz?

 

undefined.png

As per the snapshot attached, LPSPIx_SOUT  -> MOSI and LPSPIx_SIN -> MISO. Is this configuration correct or need to be reversed?

0 件の賞賛
返信
3 返答(返信)

445件の閲覧回数
Fasil1
Contributor I

Thank you for your quick reply.

Regarding ADC and PWM, we would like to know the corresponding channels that support 20kHz frequency and 400Hz frequency. 

As per the snapshot provided, it shows ADC0 has 16 channels that supports 400Hz and ADC1-2 has 4 channels that supports 20kHz. But this is not applicable to S32K312. Could you please provide the frequency of ADC and PWM channels that supports S32K312?

0 件の賞賛
返信

413件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

 

_Leo__1-1748995103790.png

Regarding the previous datasheet's screenshot, there are conditions on which the power mode tests are based. They are not specifications of the eMIOS and ADC modules as such.

eMIOS in PWM mode can archive the core frequency, which for S32K312 is 120MHz.
For ADC specifications please refer to Table 35. SAR_ADC of datasheet.

I hope this information is helpful.

Best regards,
Leonardo

0 件の賞賛
返信

471件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

SPI configuration is correct.

Regarding ADC and PWM, please provide more details about your inquiry.

Best regards,
Leonardo

0 件の賞賛
返信