S32k314 adc reading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k314 adc reading

2,262 Views
vasanth-sr
Contributor II

Hi,

i have assinged the mux_output0 pin for ADC1. the channel number is not mentioned, which channel use to read the value.

i saw in the configuration ANAMUX_OUTPUT channel. is this correct? 

Attached the screenshort.FYR.

0 Kudos
Reply
5 Replies

2,157 Views
vasanth-sr
Contributor II

Ok ,thanks

0 Kudos
Reply

2,250 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@vasanth-sr

No, for example,you can check the specific channel number like the way below.

S32K344_S32K324_S32K314_IOMUX.xlsx

Senlent_0-1682412485404.png

the PTC27->ADC1_MA[0]

S32K3XXRM_rev5: Table 295.ADC channel mapping

Senlent_1-1682412642499.png

 

0 Kudos
Reply

2,248 Views
vasanth-sr
Contributor II

Ok ,Thank you.

0 Kudos
Reply

2,228 Views
vasanth-sr
Contributor II
Hi team,

In our design, pin no 93 -ADC1_MA[0] (ADC1 -> mux_output0 -> PTC27) used to read voltage.

I configured this pin, this pin default direction is output not configurable as a input.

How can i configure and read ADC value from this ADC1_MA[0]?
0 Kudos
Reply

2,220 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@vasanth-sr

Could you please create a new question for this topic, I'm not familiar with it, thank you for your understanding

0 Kudos
Reply