S32k314 ADC reading info

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k314 ADC reading info

Jump to solution
3,311 Views
vasanth-sr
Contributor II

Hi team,

In our design, pin no 93 -ADC1_MA[0] (ADC1 -> mux_output0 -> PTC27) used to read voltage.

I configured this pin, this pin default direction is output not configurable as a input.

How can i configure and read ADC value from this ADC1_MA[0]?

0 Kudos
Reply
1 Solution
3,294 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

ADCx_MA signals are output decode signals, cannot be used as ADC input.
The ADC provides three external decode signals which it uses to select one channel out of eight in the external analog multiplexers. There can be a maximum of four such multiplexers used to connect the 32 external channels. The ADC automatically sets the decode signals to control these external analog multiplexers, based on the current external channel selected for conversion.

BR, Petr

View solution in original post

5 Replies
3,295 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

ADCx_MA signals are output decode signals, cannot be used as ADC input.
The ADC provides three external decode signals which it uses to select one channel out of eight in the external analog multiplexers. There can be a maximum of four such multiplexers used to connect the 32 external channels. The ADC automatically sets the decode signals to control these external analog multiplexers, based on the current external channel selected for conversion.

BR, Petr

2,712 Views
Agis02
Contributor I
Hi @PetrS,

Could you please mention the code to get and print temperature data for S32K314 microcontroller. Actually, very less data is available for this type of configuration.
0 Kudos
Reply
3,113 Views
EthanXu
Contributor I

So it means that all the pin connected to ADCx_MA cannot read the voltage value,right?

Tags (1)
0 Kudos
Reply
3,286 Views
vasanth-sr
Contributor II

Ok, Thank you 

0 Kudos
Reply
3,305 Views
vasanth-sr
Contributor II
Any one please help me to bringup the adc in my s32k314 platform
0 Kudos
Reply