S32k312 NvM Redundant block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k312 NvM Redundant block

1,202 Views
att919873
Contributor I

Hello,

I am trying to configure NvM redundant block with Fee reference.
Able to create a Nvm block. But it is not generating redundant fee block automatically in Fee module. I have to create it manually.
Is there any setting needs to be enabled to create a automatic redundant block in Fee?

I have attached screenshot of old project where fee redundant block is generated automatically. where AbcTest_cons0 block is generated automatically in Fee module, when I set Management type of NvM block as a redundant.

0 Kudos
Reply
3 Replies

717 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hello @att919873,

The RTD driver didn't support the NVM module, and I didn't see any note about redundant blocks in the Fee module.

Best regards,

Dan

0 Kudos
Reply

750 Views
att919873
Contributor I

@DanNguyenDuy

I am using MCal 3.0.0 Pe01 hotfix 02 RTD package...

0 Kudos
Reply

777 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hello @att919873,

What is the RTD package you are using?

Best regards,

Dan

Tags (1)
0 Kudos
Reply