Hello,
I am trying to configure NvM redundant block with Fee reference.
Able to create a Nvm block. But it is not generating redundant fee block automatically in Fee module. I have to create it manually.
Is there any setting needs to be enabled to create a automatic redundant block in Fee?
I have attached screenshot of old project where fee redundant block is generated automatically. where AbcTest_cons0 block is generated automatically in Fee module, when I set Management type of NvM block as a redundant.
Hello @att919873,
The RTD driver didn't support the NVM module, and I didn't see any note about redundant blocks in the Fee module.
Best regards,
Dan
@nxf78987
I am using MCal 3.0.0 Pe01 hotfix 02 RTD package...