S32k3 SAF for IAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k3 SAF for IAR

1,784 Views
zyt
Contributor III

Hello

I checked the SAF package of S32k3, and only found link file and startup file for gcc.

So is there .icf file and startup file can be used in IAR?

0 Kudos
Reply
3 Replies

1,761 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @zyt,

Please look into the following training for Getting Started with NXP S32 Safety Software Framework (SAF) and IAR Systems Pre-Certified Tools.

Best regards,
Julián

0 Kudos
Reply

1,713 Views
zyt
Contributor III

Hello.

The vedio mainly talk about SAF 1.0.0 with IAR, but how about the latest SAF 1.0.4?

The .icf and .s is incompatible but not provided.

0 Kudos
Reply

1,688 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @zyt,

Are you utilizing the Evaluation License? Or is this another license? The linker files are not necessarily included in the SW package, even if IAR is supported (since it's supported by the IDE in general).

Also, you can use the existing .icf linker files from the RTD installation path:

C:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Platform_TS_T40D34M40I0R0\build_files\iar

Best regards,
Julián

0 Kudos
Reply