S32k1Xx FlexIO timer 16-bit counter mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k1Xx FlexIO timer 16-bit counter mode

Jump to solution
2,010 Views
yuegao1996
Contributor II

Hi, 

   when i read S32k1 user manual, about flexio timer 16bit counter mode, it says " In 16-bit counter mode, the full 16-bits of the counter and compare register are used to configure either the baud rate of the shift clock or the shifter bit count." 

   dose it mean that the 16bit counter is FFFF at the beginning, and the timer cmp register is used for shifter bit count ?

many thanks.

0 Kudos
Reply
1 Solution
1,995 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

View solution in original post

0 Kudos
Reply
2 Replies
1,996 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@yuegao1996

    16-bit timers control the loading, shifting and storing of the shift registers, the counters load the contents of the compare register and decrement down to zero on the FlexIO clock.

 

BR!

     Jim.

0 Kudos
Reply
1,994 Views
yuegao1996
Contributor II

Thanks !

0 Kudos
Reply