Hi
S32k148HAMLU
H: 80 MHz
A: CAN FD, FlexIO, Security
S32k148UJALU
U: 112 MHz (Not valid with M temperature/125C)
J: Ethernet, Serial Audio Interface, CAN FD, FlexIO, Security (S32K148 only)
If your program does not include Ethernet, Serial Audio Interface, it may be caused by clock configuration. If you use the example where the system clock is not initialized, can you debug successfully? For example: AN5413SW\S32K1xx_cookbook\Examples\S32K148_Project\S32K148_Project_hello
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------