S32k148 supports 1588V2; PTPv2; 802.11AS(rev)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k148 supports 1588V2; PTPv2; 802.11AS(rev)?

2,131 次查看
robo
Contributor II

As you see in my question, what is supported by the S32k148?

标签 (1)
2 回复数

1,548 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

there is not direct hardware support for Precision Timing Protocol, but as you can find in reference manual, there is  Software-programmable precise time-stamping of ingress and egress frames using IEEE 1588 timer.

Please check chapter 54 in S32K1xx reference manual.

https://www.nxp.com/docs/en/reference-manual/S32K-RM.pdf 

Regards,

Martin

1,548 次查看
robo
Contributor II

Hi Martin,

thanks for the fast reply.

  • But what about chapter 54.6.10 IEEE 1588 functions? Isn't shown a HW function block with a TSU?
  • I would appreciate if you can share Information, what are the pros and cons of a SW solution compared to a HW solution?
    • Accuracy / CPU load /..

In my use-case the S32K148 shall be work as a Clock Master in gPTP Environment, synchronzied to GNSS derived pps Signal.

regards

Roland

0 项奖励
回复