Hi there ,
I am trying to find the max operating power requirement of #S32K144EVB# both interms of voltage and current. Can any one please help me out here.
cheers.
1)Powerd by 12V power source (J107 configuration 1-2)
Current limit is 250mA due to UJA1169TK spec.
2)Powerd by USB micro connector (J107 configuration 2-3)
When using USB bus power, "MIC2005-0.8YM6" on EVB is used as power switch. "MIC2005-0.8YM6" 's current limit is 0.8A.
But the current limit is 500mA due to USB spec.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------