S32k144 timer interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k144 timer interrupt

3,974 次查看
abderrahimjamao
Contributor III

Hello,

Is it possible to generate 1ms  timer interrupts using s32k144 micro?

标签 (1)
标记 (1)
1 回复

3,904 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ABDERRAHIM JAMAOUI,

Several timers can be used to generate 1ms interrupt.

User Manuals S32K1xx SDK RTM 3.0.0 with Patch 3.0.2 for ARM.png
You can refer the modification of lpit_periodic_interrupt_s32k144.

lpit_periodic_interrupt_s32k144.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------