S32k144 VDD/VDDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32k144 VDD/VDDA

跳至解决方案
1,652 次查看
lohrsistemas
Contributor IV

Hello,

Can I put:

VDD1,VDD2,VDD3,VDD4 in 3V3

and

VDDA,VREFH in 5V?

0 项奖励
回复
1 解答
1,554 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,


Is not possible to achieve what you mentioned. VDD1, VDD2, VDD3, VDD4, and VDDA must be shorted to a common source on PCB. And VREFH should always be equal to or less than VDDA + 0.1 V and VDD + 0.1 V.

So, all VDDx voltages should be equal and if VDDx is 3.3V, VREFH must not exceed 3.4V.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,555 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,


Is not possible to achieve what you mentioned. VDD1, VDD2, VDD3, VDD4, and VDDA must be shorted to a common source on PCB. And VREFH should always be equal to or less than VDDA + 0.1 V and VDD + 0.1 V.

So, all VDDx voltages should be equal and if VDDx is 3.3V, VREFH must not exceed 3.4V.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------