S32k118q048 EVB SBC programming for CAN FD messages.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32k118q048 EVB SBC programming for CAN FD messages.

135件の閲覧回数
yousefdessouki123
Contributor II

Hi,
I have an NXP S32k118q048 EVB and I want to use it to send CAN FD messages. I want to see the messages on a CANoe Vector transciever. However, I wanted to check: Do I have to porgram the SBC to get the communication active, prior to sending the CAN message. Or is the SBC already by default ready to be used for CAN messages transmission?

0 件の賞賛
返信
1 返信

110件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @yousefdessouki123,

When the board is delivered the SBC is in Forced normal mode and the CAN transceiver is enabled. No need to configure it. For more details about this mode please check UJA1169 Product data sheet, chapter 7.

Also, the UJA1169 Transceiver needs 12V power supply.

Best regards,
Julián

0 件の賞賛
返信