S32k118 ADC Accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k118 ADC Accuracy

Jump to solution
1,079 Views
종찬박
Contributor II

Hi 

I compared actual voltage to ADC value.

but, those value were quite different.

I proceeded as follows.

종찬박_0-1611623117761.png

could you tell me why calculating value is different with ADC value?

and do I have to what to check?

 

Regards,

Jongchan.

 

0 Kudos
1 Solution
1,076 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jongchan,

Please refer: AN12217, S32K1xx ADC guidelines, spec and configuration
The impedance of the analog signal source or series resistance (RIN) between the source and the input pin causes a voltage drop across it because of the current flowing into the pin. It can be understood as the resistance observed “looking out” of the ADC into the source driving the input signal to be sampled.

causes a voltage drop.png

For this reason, precautions must be taken to ensure that the analog input signal source resistance is within ADC specification. In the datasheet for S32K devices, this parameter can be found as Source Impedance (RS).Rs Source impedendance.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
434 Views
Muskz
Contributor II

Can I understand it this way? If I use an adc clock that is less than 4M, the maximum allowable rs for external circuits is 5k.
If I use an adc clock of 40M, what should be the rs? Why is it not stated in the manual, should it be larger or smaller than 5k?

Thank you.

Tags (2)
0 Kudos
1,077 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jongchan,

Please refer: AN12217, S32K1xx ADC guidelines, spec and configuration
The impedance of the analog signal source or series resistance (RIN) between the source and the input pin causes a voltage drop across it because of the current flowing into the pin. It can be understood as the resistance observed “looking out” of the ADC into the source driving the input signal to be sampled.

causes a voltage drop.png

For this reason, precautions must be taken to ensure that the analog input signal source resistance is within ADC specification. In the datasheet for S32K devices, this parameter can be found as Source Impedance (RS).Rs Source impedendance.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos