S32R294 core Z4_0:250MHZ,Z7_2 :500MHZ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R294 core Z4_0:250MHZ,Z7_2 :500MHZ

895 Views
binsan123
Contributor I

I set the clock frequency of Z4_0 core to 250Mhz, the clock frequency of Z7_2 core to 500MHZ, and the power mode to DRUN. Running the same program, it is found that the operation time of Z7_2 is longer than that of Z4_0. Normally Z7_2 should take twice as long as Z4_0. Why is this a problem?

0 Kudos
Reply
2 Replies

884 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Well that's hard to say.

In ideal cases the operation on Z7_2 at 500MHz should be faster.

But there can be different settings of buffers, access rights at memories/peripherals, wait-states at buses, etc..

To explain why it is not as you expecting will require deep knowledge on the system settings and also external signals to device.

Best regards,

Peter

0 Kudos
Reply

875 Views
binsan123
Contributor I

Thank you for your answer. My problem was solved after opening the instruction cache. By the way, it is not necessary to set part of the DRAM of S32R294 to open DCACHE and part not to open DCACHE, thank you

0 Kudos
Reply