Hi
I have a question about high voltage threshold Settings,S32M244LC‘s GDU will be closed when VSUP over 22.6V,Where can I set this value(such as set to 28V),No description of this section is found in the RM &datasheet.
thanks
解決済! 解決策の投稿を見る。
Hi Yan,
there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165). With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39
Best regards,
Pavel
Hi Yan,
there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165). With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39
Best regards,
Pavel
hi Pavel,
Thank you and regards,