S32M244LC high-voltage detect threshold

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32M244LC high-voltage detect threshold

跳至解决方案
754 次查看
YAN3
Contributor I

Hi

     I have a question about high voltage threshold Settings,S32M244LC‘s GDU will be closed when VSUP over 22.6V,Where can I set this value(such as set to 28V),No description of this section is found in the RM &datasheet.

     thanks

 

0 项奖励
回复
1 解答
729 次查看
PavelL
NXP Employee
NXP Employee

Hi Yan,

there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).  With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39

Best regards,

Pavel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
730 次查看
PavelL
NXP Employee
NXP Employee

Hi Yan,

there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).  With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39

Best regards,

Pavel

0 项奖励
回复
709 次查看
YAN3
Contributor I

hi Pavel,

   Thank you and regards,

0 项奖励
回复