S32M244LC high-voltage detect threshold

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32M244LC high-voltage detect threshold

ソリューションへジャンプ
757件の閲覧回数
YAN3
Contributor I

Hi

     I have a question about high voltage threshold Settings,S32M244LC‘s GDU will be closed when VSUP over 22.6V,Where can I set this value(such as set to 28V),No description of this section is found in the RM &datasheet.

     thanks

 

0 件の賞賛
返信
1 解決策
732件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hi Yan,

there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).  With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39

Best regards,

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
733件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hi Yan,

there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).  With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39

Best regards,

Pavel

0 件の賞賛
返信
712件の閲覧回数
YAN3
Contributor I

hi Pavel,

   Thank you and regards,

0 件の賞賛
返信