Hello,
What are the right settings of MAC Timestamp Control register in S32K344 EMAC to enable receive and transmit timestamps only for gPTP packets?
Thank you,
Jakub
Hello Jakub,
I supposed so. However, the EMAC only captures TX/RX timestamp and store in the relative descriptor. Maybe you will need some more SW implementations in order to fulfil the gPTP stack.
Best Regards,
Nam
Hi Nam,
Yes, for sure SW stack is needed.
Best regards,
Jakub
Hello,
802.AS mode can be enabled by setting 1 to MAC_Timestamp_Control[AV8021ASMEN] register.
Best Regards,
Nam
Hi Nam,
Thank you for the answer.
Is this the only bit that needs to be set in the register to enable rx/tx timestamps only for gPTP (802.1AS) frames or other fields need to be set as well?
Best regards,
Jakub