After installing the S32K3xx development package when using S32DS3.4 on Ubuntu, I can see the folder ./S32DS.3.4/S32DS/software/PlatformSDK_S32XX_2022_03 and I can select that platform SDK when starting a project using the S32K344.
However, after installing S32DS3.5 and installing the S32K3xx development pacakge, I do not see the software directory ./S32DS.3.5/S32DS/software and I cannot select an SDK for the S32K344.
Am I doing something wrong?
Trying the same thing on Windows 11 (using S32DS3.5 with the S32K3xx development package) it installs correctly.
Well, this is not documented appropriately. Current SDK and RTD packages are not supported in Linux. It was discussed several times here on the community. For example:
https://community.nxp.com/t5/S32-Design-Studio/S32K3-SDK-Re-Attach-RTD-SDK-from-command-line/m-p/146...
I was told there’s a plan to support RTD in Linux and currently it looks like it will be available in next version of S32 Design Studio 3.6.
Sorry for inconvenience.
Regards,
Lukas