S32K3xx: S32DS Platform IDE: Change controller for an existing S32DS project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3xx: S32DS Platform IDE: Change controller for an existing S32DS project

ソリューションへジャンプ
505件の閲覧回数
tecprasant
Contributor II

Hi,

I have used S32DS Platform IDE and created a project for S32K3x4 IC. I would now like to change this project to S32K31x controller.

What is the best way to update an existing project? 
Is there any document highlighting the steps required to make this change?

 

I want to avoid creating a fresh project from scratch.

 

Any inputs will be of help.

 

Regards

タグ(3)
0 件の賞賛
返信
1 解決策
480件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

Currently, the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best regards,
Julián

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
411件の閲覧回数
tecprasant
Contributor II

Thanks @Julián_AragónM . This information makes it very clear for me.

481件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

Currently, the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best regards,
Julián

0 件の賞賛
返信
423件の閲覧回数
tecprasant
Contributor II

@Julián_AragónM : Thanks for the inputs. This answers my query.

I have an additional query: If I want to only change the MCU package, say from S32K344 172 pin package to 100 pin package, then what is recommended?
(a) I create a new project?
(b) I change the package in the NXP package selection (in the same project) ?

 

Regards,

0 件の賞賛
返信
417件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @tecprasant,

For changing the package, this can be done inside the S32DS Config Tool (option b), just keep in mind the difference between these packages and modify the pin configurations accordingly.

Julin_AragnM_0-1715702816302.png

Best regards,
Julián

0 件の賞賛
返信