[S32K3xx] - Program a byte in UTEST sector

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K3xx] - Program a byte in UTEST sector

跳至解决方案
6,835 次查看
atranzillo93
Contributor III

Hi,

I'm trying to write a byte in UTEST sector in this block:

atranzillo93_0-1700150357982.png

NB: API is called at init with interrupts disabled.

 

This is my code:

 HostFlash_Program((uint32_t )0x1B000780U, (uint8_t* )hseFwFeatureFlagEnabledValue, (uint32_t)8U);

eel_status_t HostFlash_Program( uint32_t Address, uint8_t* SourceAddress, uint32_t Length)
{
uint32_t ErrorFlags;
C40_Ip_StatusType C40_Ip_Status = STATUS_C40_IP_ERROR ;
const uint8_t *DataPtr8 = SourceAddress;
volatile uint32_t DataTemp32; /* Prevent compiler optimization when working with unaligned addresses */


/* Disable HV to finalize/abort the operation */
Fsld_FlashInstance->MCR &= ~FLASH_MCR_EHV_MASK;
/*Clear ERS and PGM bits */
Fsld_FlashInstance->MCR &= ~(FLASH_MCR_PGM_MASK|FLASH_MCR_ESS_MASK|FLASH_MCR_ERS_MASK);
/* Disable watchdog interrupt */
Fsld_FlashInstance->MCR &= ~FLASH_MCR_WDIE_MASK;
/* No interrupt request will be generated when the DONE flag is set */
Fsld_FlashInstance->MCR &= ~FLASH_MCR_PECIE_MASK;
/* Clear all error flags for main interface */
Fsld_FlashInstance->MCRS &= FLASH_MCRS_EER_MASK | \
FLASH_MCRS_SBC_MASK | \
FLASH_MCRS_AEE_MASK | \
FLASH_MCRS_EEE_MASK | \
FLASH_MCRS_RVE_MASK | \
FLASH_MCRS_RRE_MASK | \
FLASH_MCRS_RWE_MASK | \
FLASH_MCRS_PES_MASK | \
FLASH_MCRS_PEP_MASK;


/* Sector is in Utest */
Fsld_PFlashInstance->PFCBLKU_SPELOCK[0u] &= FSLD_MASK_UNLOCK_UTEST_SECTOR;

/* Write the address to be programmed */
Fsld_PFlashInstance->PFCPGM_PEADR_L = Address;

DataTemp32 = (uint32_t)DataPtr8[0U] << 0U;
DataTemp32 |= (uint32_t)DataPtr8[1U] << 8U;
DataTemp32 |= (uint32_t)DataPtr8[2U] << 16U;
DataTemp32 |= (uint32_t)DataPtr8[3U] << 24U;
Fsld_FlashInstance->DATA[0U] = DataTemp32;

DataTemp32 = (uint32_t)DataPtr8[4U] << 0U;
DataTemp32 |= (uint32_t)DataPtr8[5U] << 8U;
DataTemp32 |= (uint32_t)DataPtr8[6U] << 16U;
DataTemp32 |= (uint32_t)DataPtr8[7U] << 24U;
Fsld_FlashInstance->DATA[1U] = DataTemp32;

/* Setup program operation */
Fsld_FlashInstance->MCR |= FLASH_MCR_PGM_MASK;
/* Start internal erase/program sequence */
Fsld_FlashInstance->MCR |= FLASH_MCR_EHV_MASK;

while (0U == ((Fsld_FlashInstance->MCRS & FLASH_MCRS_DONE_MASK) >> FLASH_MCRS_DONE_SHIFT))
{

}

ErrorFlags = Fsld_FlashInstance->MCRS & (FLASH_MCRS_PEG_MASK | FLASH_MCRS_PEP_MASK | FLASH_MCRS_PES_MASK);
/* Program/Erase Good: only PEG = 1; both PEP and PES should be 0 */
if (FLASH_MCRS_PEG_MASK == ErrorFlags)
{
C40_Ip_Status = STATUS_C40_IP_SUCCESS;
}
else
{
C40_Ip_Status = STATUS_C40_IP_ERROR;
}

/* terminate program operation */
Fsld_FlashInstance->MCR &= ~FLASH_MCR_EHV_MASK;
/* Terminate program operation */
Fsld_FlashInstance->MCR &= ~FLASH_MCR_PGM_MASK;


/* The write job has finished or the end of the sector was reached. Time to lock the sector */
Fsld_PFlashInstance->PFCBLKU_SPELOCK[0u] |= FSLD_MASK_LOCK_UTEST_SECTOR;

if( STATUS_C40_IP_SUCCESS == C40_Ip_Status )
{
return EEL_OK ;
}
else
{
return EEL_ERR_PARAMETER ;
}
}

 

  • #case1

If I don't place the function in RAM, it writes the byte but, just after the write uC generates a hard fault

atranzillo93_1-1700150470064.png

#case 2

If I place the function in RAM, no hard fault occurs, but write operation fails. Byte is not written in UTEST sector.

atranzillo93_2-1700150752156.png

 

Can you help me?

 

Thanks a lot.

标记 (1)
0 项奖励
回复
1 解答
6,233 次查看
atranzillo93
Contributor III

SOLUTION:

I have separated the setting of PGM and EHV bits in two differents API.

在原帖中查看解决方案

0 项奖励
回复
12 回复数
6,234 次查看
atranzillo93
Contributor III

SOLUTION:

I have separated the setting of PGM and EHV bits in two differents API.

0 项奖励
回复
6,807 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @atranzillo93 

The UTEST Sector is an OTP (One Time Programmable). This causes the erase operations not to be allowed. You only going to be able to append new data or configuration and read data.

Writing the desired data in the UTEST Sector is the same process used to program data in other blocks.

Please check the following post. Is from other topics but explains how to write data in a UTEST sector. 

[S32K3] Restrict the debug access with a password when HSE is not used

 

B.R.

VaneB

0 项奖励
回复
6,795 次查看
atranzillo93
Contributor III

Hi vanessa,

I have tried your same code, the write in UTEST is correctly performed but just after the write uC goes in hard fault:

eel_status_t HostFlash1_Program(void)
{
C40_Ip_StatusType flashStatus;
uint32_t DcfRecord[2] = {0x00000100, 0x00100004};
/* If the target address is un-programmed state, start the programming process. */
if( (*(uint32_t *)0x1B000770 == 0xFFFFFFFF) && (*(uint32_t *)(0x1B000770+4) == 0xFFFFFFFF) )
{
/* Must unlock the UTEST Flash area before programming. */
Fsld_PFlashInstance->PFCBLKU_SPELOCK[0u] &= 0xFFFFFFF0U;

/* Write the new DCF records into UTEST Flash. */
flashStatus = C40_Ip_MainInterfaceWrite(0x1B000770, 8, (uint8_t *)(&DcfRecord[0]));
/* Cache_Ip_CleanByAddr(CACHE_IP_DATA, TRUE, TargetAddress, 8); */

/* Poll the Flash status until the programming sequence is done. */
do {
flashStatus = C40_Ip_MainInterfaceWriteStatus();
}while(STATUS_C40_IP_SUCCESS != flashStatus);

/* Must lock the UTEST Flash area after programming. */
Fsld_PFlashInstance->PFCBLKU_SPELOCK[0u] |= 0x0000000FU;
}

if( STATUS_C40_IP_SUCCESS == flashStatus )
{
return EEL_OK ;
}
else
{
return EEL_ERR_PARAMETER ;
}
}

 

atranzillo93_0-1700215264747.png

 

Can you explain me why?

 

Best regarsds, Anna

0 项奖励
回复
6,787 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @atranzillo93 

Does the MCU go to Hard Fault when you lock the UTEST sector? Or does this happen when the MCU terminates the ostFlash1_Program(void)?

0 项奖励
回复
6,725 次查看
atranzillo93
Contributor III

Hi vanessa,

 

the MCU goes in hard fault when calls the API:

flashStatus = C40_Ip_MainInterfaceWriteStatus();

 

Best regards,

Anna

0 项奖励
回复
6,712 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @atranzillo93 

As mentioned, the UTEST Sector is an OTP (One Time Programmable). So, if you already write data in an address, you cannot append new data or configuration. 

If the first time the data was written successfully, if you run the code, it causes a hard fault because that address is no longer accessible for writing. 

0 项奖励
回复
6,707 次查看
atranzillo93
Contributor III

Hi Vanessa

address where I try to write is empty, so I CAN write.

The data are effectively written but during the read of Write status (DONE bit) an hard fault occurs.

I hope to be clear now.

See the images that I have attached to issue, please.

Anna

0 项奖励
回复
6,704 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @atranzillo93 

Could you please verify if this behavior also presents with the C40_Ip_Example?

0 项奖励
回复
6,701 次查看
atranzillo93
Contributor III

Ok ,I will verity it.

0 项奖励
回复
6,832 次查看
atranzillo93
Contributor III

The hard fault generates here:

atranzillo93_0-1700151260382.png

 

标记 (1)
0 项奖励
回复
6,522 次查看
BhushanM
Contributor II

I faced same issue. controller was going to hard fault for both RAM and Flash region execution.

I tried adding 5ms delay inside "C40_Ip_MainInterfaceWrite" function. please refer from below.

if (TRUE == C40_Ip_bAsync)
{
/* Start flash access */
C40_Ip_FlashAccessCalloutStart();
HAL_DelayMs(5);
/* Start internal erase/program sequence */
C40_Ip_pFlashBaseAddress->MCR |= FLASH_MCR_EHV_MASK;
HAL_DelayMs(5);
}

its working for me, executing from flash region.

 

 

 

0 项奖励
回复
6,299 次查看
atranzillo93
Contributor III

Hi,

delay doens't solve the hard fault in my application.

Do you have any suggests?

 

Best regards,

Anita

0 项奖励
回复