I used the example project Eth_InternalLoopback_Q172_S32K344 in compiler S32DS 3.4.3 and found DMA could not be reset in function Gmac_Ip_InitDMA (Gmac_Ip.c:391),Whether this sample project requires additional Settings? I expect Ethernet data to be sent and received through the board(S32K344EVB-Q172) chip DP83848C, is there a corresponding example project?
Hello,
In order to run the example, did you follow with the description in the readme.txt file?
Unfortunately, there is no example for external communication.
Best Regards,
Nam