S32K3x4-Q172 EthDemo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3x4-Q172 EthDemo

441件の閲覧回数
darrenZhk
Contributor I

I used the example project Eth_InternalLoopback_Q172_S32K344 in compiler S32DS 3.4.3 and found DMA could not be reset in function Gmac_Ip_InitDMA  (Gmac_Ip.c:391),Whether this sample project requires additional Settings? I expect Ethernet data to be sent and received through the board(S32K344EVB-Q172) chip DP83848C, is there a corresponding example project?

0 件の賞賛
1 返信

411件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

In order to run the example, did you follow with the description in the readme.txt file?

Unfortunately, there is no example for external communication.

Best Regards,

Nam

0 件の賞賛