S32K3X4EVB-T172 UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3X4EVB-T172 UART

Jump to solution
657 Views
jacob_ala
Contributor I

Hello! We're looking at testing with the S32K3X4EVB-T172 Evaluation Board for development of a custom automotive controller. How many UART peripherals are supported by this evaluation board?

Thank you!

0 Kudos
Reply
1 Solution
643 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jacob_ala 

As shown in the below image, S32K314, S32K324 and S32K344 has 15 UART instances. Also, you can refer to the S32K344_S32K324_S32K314_IOMUX.xlsx file attached to the RM to see the pins that can be configured for each UART. 

VaneB_0-1678828334819.png

 

B.R

VaneB

 

View solution in original post

0 Kudos
Reply
2 Replies
644 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jacob_ala 

As shown in the below image, S32K314, S32K324 and S32K344 has 15 UART instances. Also, you can refer to the S32K344_S32K324_S32K314_IOMUX.xlsx file attached to the RM to see the pins that can be configured for each UART. 

VaneB_0-1678828334819.png

 

B.R

VaneB

 

0 Kudos
Reply
640 Views
jacob_ala
Contributor I
Perfect, thank you! As long as all those pins are accessible on the Evaluation Board, then it should work! Cheers
0 Kudos
Reply