S32K3X4EVB-Q257

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3X4EVB-Q257

238件の閲覧回数
xuan
Contributor I

HI,

I am using the S32K3X4EVB-Q257 development board, I encountered the following problem when debugging: In the process of using the PE downloader Debug prompt: flash programming error. Terminating the debug session.

I want to know what I need to do to Debug the program normally?

xuan_0-1719812422511.png

I am using routines imported from the official library

xuan_1-1719812546878.png

 

 

0 件の賞賛
返信
1 返信

216件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @xuan 

The example codes are provided to run out of the box and are compatible with S32K3X4EVB-Q257 and S32K3X4EVB-Q172. No changes are necessary.

Make sure the board is powered by a 12V power supply, the jumpers are set correctly, and the debugger is detected by the computer. I am attaching some links to documents that may be useful.

Getting Started with the S32K3X4EVB-Q257 Evaluation Board

S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual

 

B.R.

VaneB

0 件の賞賛
返信