HI,
I am using the S32K3X4EVB-Q257 development board, I encountered the following problem when debugging: In the process of using the PE downloader Debug prompt: flash programming error. Terminating the debug session.
I want to know what I need to do to Debug the program normally?
I am using routines imported from the official library
Hi @xuan
The example codes are provided to run out of the box and are compatible with S32K3X4EVB-Q257 and S32K3X4EVB-Q172. No changes are necessary.
Make sure the board is powered by a 12V power supply, the jumpers are set correctly, and the debugger is detected by the computer. I am attaching some links to documents that may be useful.
Getting Started with the S32K3X4EVB-Q257 Evaluation Board
S32K3X4EVB-Q257 and Q257ND Evaluation Board – HW User Manual
B.R.
VaneB