S32K358 IPCF example build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K358 IPCF example build error

3,678 次查看
FLolli
Contributor I

I am in development of a multicore FreeRTOS application on s32K358 and i am trying to compile IPCF 4.0.0 D2306 Example project on S32DS 3.5 Build ID 230629 (Update3). I have followed compatible software suggestion in the release note and as far as i know i am compliant with it. 

After source code generation and build i get following error

#error "ipc-shm.h and ipcf_Ip_Cfg.h have different vendor IDs"

on both header files of both projects (Core0 and Core2).

it seems that IPC_SHM_VENDOR_ID 43 and IPCF_IP_CFG_VENDOR_ID_C 40 are incompatible but i have no idea of where to check those infos since code is autogen.

attached you can find my installation details since i think it may be related to S32DS configuration. 

Thanks in advance for the help

标记 (1)
1 回复

3,576 次查看
NamLee
NXP Employee
NXP Employee

Hi FLolli,

After discussing with our teams, I think this maybe a bug.

The expectation of vendor id value is 43. Please help me to workaround this issue by changing values to 43.

I already raised ticket and expect that it'll be fixed in the next release.

Thank you so much for reporting this issue.

Thank you,

Nam.