S32K358 Can example Build Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K358 Can example Build Error

960 次查看
WKL
Contributor I

We are working on a project using NXP S32K358 MCU. As a staring point I tried to run CAN example from SDK. I imported the project from NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Can_43_FLEXCAN_TS_T40D34M40I0R0\examples\S32DS and updated code based on the configurations provided by the example. But it failed the build with such errors:

WKL_0-1704744381118.png

Any ideas why it failed and is there anything I missed for the example project?

We used 3.5 for S32 Deign Studio.

BTW, I just imported another example (I2c_Example_S32K358) and it built successfully. So the build errors may be just related to CAN example?

Thanks!

 

0 项奖励
回复
1 回复

952 次查看
WKL
Contributor I

Fixed the issue by click project->manage SDK and restored the missing files.

0 项奖励
回复