S32K358 BMU Time out issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K358 BMU Time out issue

1,311件の閲覧回数
mishra1
Contributor I

Hi,

 

I am using HVBMS 800BUN with ETPL. I am made a observation that the data at Freemaster comes only for 20-22 minutes. Even the BJB led goes off.

I am not sure is it only because of communication issue at Freemaster or some design/driver code issue?

 

Would be glad if someone can help me with this issue?

 

Regards,

Sonu

0 件の賞賛
返信
3 返答(返信)

1,278件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Which example are you running?
D1 LED\RED (VCOM_PRIM) on the RD772BJBTPL8EVB board is not light? The engineer responsible for MC33772C told me that it looks like the MC33772C is in Sleep/Idle mode:

Table 12. Power supply mode operation.png

Also, which debugger are you using? Perhaps you can use the following method to observe which step the program is running to: Connecting to a running Target (attach) with S32 Design Studio for S32 Platform 3.3

Due to the Christmas vacation period, our response times may be longer than usual. We appreciate your patience as our team navigates this busy season. 
Please be assured, we are committed to responding your inquiries as quickly as possible. 
Thank you for your understanding and happy holidays!

Best Regards,
Robin

0 件の賞賛
返信

1,258件の閲覧回数
mishra1
Contributor I

Hi Robin,

 

I am running HvBms800_774_772_TPL_Bring_Up project.

I am controlling Contactors in normal mode(which is the ideal scenerio).

In normal mode, I am getting values through Freemaster for 20 minutes approx. After 20 mins, the blinking LED in BMU goes off and the LED on BJB also goes off.

 

Note: I am using DEMO version of HvBMS TPL project.

 

My question is: In the Demo project, does the driver configuration supports only for few cycles? Or am I missing something?

 

Regards,

Sonu

タグ(1)
0 件の賞賛
返信

1,212件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I searched but couldn't find the reason.
Have you modified HvBms800_774_772_TPL_Bring_Up and the hardware?
Also, you haven't told me what you see if you connect the program with a debugger. Did you check which error flags are set?
If nothing is found, I'm afraid I'll have to consult the HVBMS software team for more help.

0 件の賞賛
返信