Hi @Shivanand
I have compared the packages you have installed with my environment, and I noticed that some of your packages are not up-to-date. To rule out any potential issues caused by this, could you please update the packages I have highlighted in yellow?
Once you have done that, kindly let me know if you observe any changes in the project.
Hi @Shivanand
Usually, the "no such file or directory" error is caused by a missing configuration. In most cases, before running the example, a configuration needs to be generated. To do this, follow these steps:
Additionally, please verify if the include file path contains any extra spaces or if the issue is caused by missing RTD/SDK installation or incorrect user configuration. To check this:
Ensure that the file paths are correct and do not contain unnecessary spaces.
BR, VaneB
Hi @Shivanand
The BESS demo application comes with a file listing all the required software dependencies. Could you please confirm if all of these dependencies have been installed in your S32DS instance?
Hi @Shivanand
I have not been able to reproduce the error you are encountering, but I have made some important modifications that allow the S32K3-BESS-Firmware-Version-0.8.0-Demo to compile without any issues. Please follow the changes below and let me know if this resolves your problem:
Hi @VaneB. The error I'm getting is different; I'm posting an image of errors. There are two reference applications, 0 & 2. Application_2 is built, but application_0 has errors
Hi @Shivanand
Could you please provide your S32DS installation details? I want to verify if there are any conflicts between packages or if there are any missing packages that could be causing the error you are experiencing.
Hi @VaneB Installation Details
Package: S32 Design Studio Platform package; Version: 3.5.14; Build id: 202409241924
Package: S32K3 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Package: SW32K3 IPCF 4.0.0 D2306; Version: 4.0.0; Build id: 202306301110
Package: HB200X for S32K3XX; Version: 0.8.0; Build id: 202307140229
Package: S32K3xx development package; Version: 3.5.0 RTM; Build id: 202304051438
Package: S32K396 development package; Version: 3.5.0 EAR2; Build id: 202209290838
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202109281337
Package: TCPIP_STACK for S32K3 version 1.0.3; Version: 1.0.3; Build id: 202306190957
Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521
Package: GDB Client for Arm Embedded Processors 12.1 Build 1702; Version: 1702; Build id: 202309251304
Package: FS26 for S32K3 version 2.0.0; Version: 2.0.0; Build id: 202308040805
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202005201157
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.5.7; Build id: 202304031909
Package: S32K3 SAF_EVAL RTM 1.0.4; Version: 1.0.4; Build id: 202312210949
Package: SW32K3 BMS SDK Autosar 4.4 R21-11 Version 1.0.1; Version: 1.0.1; Build id: 202308301443
Package: FreeRTOS for S32K3 3.1.0; Version: 3.1.0; Build id: 202304240736
Package: S32 Design Studio Platform Tools package; Version: 3.5.11; Build id: 202403280939
Package: SW32K3 BMS SL SDK Autosar 4.4 R21-11 Version 1.0.1 DEMO; Version: 1.0.1; Build id: 202308301406
Package: S32K396 RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Package: S32 Design Studio Debugger Core; Version: 3.5.11; Build id: 202403271836
Package: S32K3XX RTD AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202303311831
Hi @Shivanand
I have compared the packages you have installed with my environment, and I noticed that some of your packages are not up-to-date. To rule out any potential issues caused by this, could you please update the packages I have highlighted in yellow?
Once you have done that, kindly let me know if you observe any changes in the project.