S32K34x Low power mode result

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K34x Low power mode result

Jump to solution
668 Views
OliverTian
NXP Employee
NXP Employee

Hello, 
    Based on the minimum system board (all IOs are floating) of S32K34x, the low power mode result is as Datasheet.
    Hope will be helpful for you as reference. 

OliverTian_0-1689053536546.png
Cheers !
Oliver

 



0 Kudos
1 Solution
667 Views
OliverTian
NXP Employee
NXP Employee

S32K3 mini EVB:

* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;

View solution in original post

0 Kudos
1 Reply
668 Views
OliverTian
NXP Employee
NXP Employee

S32K3 mini EVB:

* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;

0 Kudos