S32K344 Whiteboard Example Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K344 Whiteboard Example Project

跳至解决方案
12,565 次查看
StephenDu
NXP Employee
NXP Employee

@S32kUser 

The S32K344 Whiteboard (S32K344-WB) is a reference design board for providing quick prototype verification, such as Body Domain Control, Gateway, Passive Entry Passive Start (PEPS), Motor Control, and so on. It Based on the 32-bit Arm® Cortex®-M7 S32K3 MCU in a 257 MPABGA package.
To help customers get familiar with the hardware quickly, a set of example projects are provided based on the Real-Time Drivers(RTD) provided by NXP. With these example projects, you can have an out-of-box experience with the S32K344-WB reference design. You can get this example package from the attachment on this page.

nxf50137_0-1659597023656.png

 

标记 (3)
1 解答
12,564 次查看
StephenDu
NXP Employee
NXP Employee

To get more example projects for S32K344-WB, please contact me.

在原帖中查看解决方案

0 项奖励
回复
22 回复数
1,517 次查看
ekmas-19
Contributor II

Hi Stephen,

Can you provide an example using half Duplex Lpspi and for Qspi_lp? I would like to see how they are configured and used for the S32K344-WB board. 

Preferably for a bare metal application.

Thanks! 

0 项奖励
回复
1,490 次查看
ekmas-19
Contributor II
Is there an LLD Driver API? I have searched the website, and the S32DS help content. I cannot find one.
There is one for the mcuxpresso drivers, but these are different than what gets generated from RTD libraries with the Eclipse IDE.
0 项奖励
回复
10,353 次查看
StephenDu
NXP Employee
NXP Employee

We have provided a richer sample project. Please take it if you needed.

0 项奖励
回复
9,638 次查看
GavinLi1
Contributor III

Thanks for the info!

I have build errors when import the examples, shows at:

GavinLi1_0-1704453986437.png

Also, I import the EB project, shows error:

GavinLi1_1-1704454031885.png

 

Anything else I miss?

The S32DS  version:

S32 Design Studio for S32 Platform
Version: 3.5
Build id: 231128 (Update

 

Is it ok to compile the examples?

 

Thanks in advance!

Gavin

0 项奖励
回复
9,633 次查看
GavinLi1
Contributor III

I checked that again, it seems the issue for the EB.

I re-installed it and it's ok now. Projects can be built pass.

0 项奖励
回复
12,403 次查看
StephenDu
NXP Employee
NXP Employee

To get more Multi-Core example projects, please switch to the page: S32K324 Multi-Core Example Project based on Whiteboard

0 项奖励
回复
12,565 次查看
StephenDu
NXP Employee
NXP Employee

To get more example projects for S32K344-WB, please contact me.

0 项奖励
回复
8,477 次查看
yomna_attia
Contributor I

Hello, 

Could you send me an example for client program, such as SocketTest, for the S32K344 WHITEBOARD?

Thanks in advance, 

0 项奖励
回复
8,455 次查看
StephenDu
NXP Employee
NXP Employee

hi, Yomna

Due to this is a third-party software (Not sure the license limitation), please download by yourself. I can only to tell you the name which we are using: Wireshark.

0 项奖励
回复
8,445 次查看
yomna_attia
Contributor I

I mean what are the steps to configure the ethernet example for the S32K344 WB to be client (use the Socket example as Client ).

 Thanks in advance .

0 项奖励
回复
8,498 次查看
yomna_attia
Contributor I

I tried to reconfigure the LWIP example to be CLient but i faced this lwip_connect function returns error out of memory and i don't know why this happen so if you have a client example working properly could you you sent it to me

Thanks in advance 

0 项奖励
回复
8,551 次查看
Mossab
Contributor I

Hi, 

would you please send me TCP/IP example that compatible with the mentioned board

0 项奖励
回复
8,527 次查看
StephenDu
NXP Employee
NXP Employee

hi, Mossab

The TCP/IP (LWIP) only has the LLD version, it is included in the S32K344_Whiteboard_Example(LLD)_RTM_1.0.0.zip attached in this page, please download and install it (Above this message).

0 项奖励
回复
8,616 次查看
yomna_attia
Contributor I
I want LWIP example
0 项奖励
回复
8,581 次查看
StephenDu
NXP Employee
NXP Employee

hi, Yomna

The LWIP only has the LLD version, it is included in the S32K344_Whiteboard_Example(LLD)_RTM_1.0.0.zip attached in this page, please download and install it (Above this message).

0 项奖励
回复
8,579 次查看
yomna_attia
Contributor I

I already checked it and i found the lwip example thank you for your support 

I also have another question is this example client or server and what's the configured ip address

0 项奖励
回复
12,254 次查看
daich
Contributor I

I use s32k344 now, and i want to get some IAR project.

how to get it? thank you very much!

0 项奖励
回复
12,236 次查看
StephenDu
NXP Employee
NXP Employee

hi,

In the attachment, there is include one IAR example project which located in the IAR folder. You can create your own project based on this example project.

0 项奖励
回复
12,317 次查看
savantwxj
Contributor I

Hi 

Would you help provide the mcal eb project of this S32K344 Whiteboard? I will use it as a starting point of my own mcal eb project based on our own HW board. Thanks!

0 项奖励
回复
12,296 次查看
StephenDu
NXP Employee
NXP Employee
hi, savantwxj In fact, it is there. Please refer to the "Tresos_Project" folder in each example project.
0 项奖励
回复